Fort Worth, Texas – November 3, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the VCNL4035 family of Proximity Sensors from Vishay. These sensors are targeted to meet the requirements of various medical, process automation and industrial applications.

Vishay’s VCNL4035X01 integrates a proximity sensor (PS), ambient light sensor (ALS), a muxx and a driver for up to 3 external IREDs / LEDs into one small package. It incorporates photodiodes, amplifiers and analog-to-digital converting circuits into a single chip by CMOS process. The 16-bit high resolution ALS offers excellent sensing capabilities with sufficient selections to fulfill most applications whether dark or high-transparency lens design. Both ALS and PS programmable interrupt features of the individual high and low thresholds offer the best utilization and power savings on the microcontroller. The Proximity Sensor features an intelligent cancellation scheme, so that cross talk phenomenon is eliminated. To accelerate the PS response time, smart persistence prevents the misjudgment of proximity sensing but also keeps a fast response time. Active force mode, one time trigger by one instruction, is another good approach for more design flexibility to fulfill different kinds of applications with more power savings in battery-powered applications.

To learn more, visit Vishay Proximity Sensors at TTI

About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com.