Fort Worth, Texas – May 19, 2020 –  TTI, Inc., a leading specialty distributor of electronic components, is now stocking TE Connectivity’s new DOG2 MEMS Series CAN J2939 dual axis inclinometer.

TE Connectivity’s (TE) DOG2 MEMS Series CAN J1939 dual-axis inclinometers can simultaneously measure pitch and roll angles of up to ±90°, with <0.5% of cross-axis sensitivity (versus the 1 to 2 percent industry standard). On-board linearization and temperature compensation result in an extremely low total output error of 0.5°, over a wide -40° to +85°C operating temperature range. Integrated digital filtering algorithms limit the effects of vibrations and/or shock. The digital output eliminates errors such as noise and signal loss common to analog type sensors. A high impact plastic housing and IP67 rating provide excellent protection in harsh environments where condensation, oils, grease, fuels and other contaminants may be present.

Applications include: stability control for off road vehicles, agricultural equipment, man lifts and lift platforms, and crane manufacturers.

To learn more, or check our available stock, visit the TE DOG2 MEMS Tilt Sensors product page.

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com

About TE Connectivity’ Sensor Solutions

TE Connectivity Ltd. (NYSE: TEL) is a $13 billion global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions, proven in the harshest environments, enable advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With nearly 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 150 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at http://www.te.com/ and on LinkedIn, Facebook, WeChat and Twitter.