Fort Worth, Texas – May 11, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now offering the OPB856Z Wide Gap Sensors from Optek. These sensors are targeted for medical and industrial applications where object movement and detection are critical.
The OPB856Z emitter and sensor pair consists of an LED (935 nm) and a Phototransistor designed for optimum coupling efficiency with each other. They are mounted in a threaded (M12x1TH) color-coded housing. The LED (white) and the Phototransistor (black) are designed to easily panel mount in through a 0.4724” (12.0 mm) hole. A 12 mm nut is included for each housing. Both components are designed to interconnect with a Molex (03-06-2023) connector.
The OPB856Z sensor pair is perfect for medical and industrial equipment applications in detection of object presence, movements or location. This sensor pair is designed to operate with separation distances between the LED and Phototransistor up to 12” (30.48 cm). Sensor is constructed with a very robust design to survive harsh environments.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com
About TT Electronics
TT Electronics is a focused, global electronics group supplying products to leading manufacturers in the defense and aerospace, medical, transportation, energy and industrial electronics markets. The TT electronics technology portfolio is one of the most comprehensive in the industry, supplying passive components (fixed and variable resistors, magnetics) and discrete semiconductors (optoelectronics, diodes, MOSFETs) from brands including BI Technologies, IRC, Optek, Semelab and Welwyn Components. TT Electronics is continually investing in new product development, supported by world class application.