Fort Worth, Texas – May 8, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now offering TE Connectivity’s HTU31 humidity and temperature combination sensor. TE Connectivity has designed the HTU31, one of the smallest and most accurate humidity sensors on the market. The HTU31 provides fast response time, precision measurement, low hysteresis and sustained performance even when exposed to extreme temperature (-40° to 125°C) and humidity environments (0%-100%). ​

The HTU31 humidity sensor includes both digital (D) and analog (V) versions, and combines multiple functions and various interfaces (I²C, analog, voltage output) with an application-friendly operating voltage range (3.3-5.5V with 5V typical) and a small footprint of 2.5 x 2.5 x 0.9mm.

To learn more about this product, visit the TE Humidity/Temp Sensor page. 

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains over 2 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 7,000 people at more than 133 locations throughout North America, South America, Europe, Asia and Africa. For more information about TTI, visit www.ttiinc.com