Fort Worth, Texas – October 23, 2019 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking the OPB9001 reflective optical sensor module from TT Electronics. This sensor is targeted for medical and industrial applications including industrial printing, asset tracking, factory automation, automated banking systems, safety and security devices, and portable medical equipment.

The OPB9001 is a reflective, CMOS logic output sensor with programmable sensitivity, incorporated into a module assembly offering voltage protection, output calibration, temperature compensation, and multifunction indicator LEDs. This unit is factory calibrated for a 12mm distance on a white reflective card. The OPB9001 can be recalibrated with a single command for unique applications or surfaces ranging from 2.5mm to 50mm. The operational supply voltage can range from 3.3V to 30V. The industry-leading response time of 6µs ensures high-speed detection for time-critical applications. Excellent ambient light immunity along with 8kV ESD protection sets the OPB9001 apart from the competition.

Learn More

 

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, South America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com

About TT Electronics

TT Electronics is a focused, global electronics group supplying products to leading manufacturers in the defense and aerospace, medical, transportation, energy and industrial electronics markets. The TT Electronics technology portfolio is one of the most comprehensive in the industry, supplying passive components (fixed and variable resistors, magnetics) and discrete semiconductors (optoelectronics, diodes, MOSFETs) from brands including BI Technologies, IRC, Optek, Semelab, and Welwyn Components. TT Electronics is continually investing in new product development, supported by world-class application engineering teams committed to understanding and fulfilling customer needs with innovative technology.

TT Electronics Optical Sensor