Fort Worth, Texas – May 14, 2019 – TTI, Inc., the leading specialty distributor of electronic components, now has in stock the CII FCC-360 60-Amp contactor from TE Connectivity. The contactor’s 2.5” x 2.1” footprint packs high-performance and durability into a small case size. The component features a rugged double make contact design, reduces wear and tear for long life, and the gasket seal allows it to stand up to tough military, aerospace and marine environments. The fast switching contactor is designed for easy installation and to meet the performance specifications of MIL-PRF -6106.
As an AS9100D and ISO 9001 certified distributor, TTI stocks the CII FCC 360 for use in military aircraft, UAVs, commercial aerospace applications, military ground equipment, and shipboard electronics.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group, TTI employs more than 6,700 people at more than 133 locations throughout North America, Europe, and Asia. For more information about TTI, visit www.ttiinc.com
About TE Connectivity
TE Connectivity Ltd. (NYSE: TEL) is a $14billion global technology and manufacturing leader creating a safer, sustainable, productive, and connected future. For more than 75 years, our connectivity and sensor solutions, proven in the harshest environments, have enabled advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat and Twitter.