Capacitors have resistance in their electrodes and dielectrics. This resistance generates heat when AC current like ripple current – a periodic non-sinusoidal waveform derived from an AC power source – passes through.
Capacitors are rated for ripple current and exceeding the ripple current rating will increase internal heating, limit the overall reliability of the device and reduce the capacitor’s lifetime. High ripple current and high temperature of the environment in which the capacitor operates causes heating due to power dissipation. High temperatures can also cause hot spots within the capacitor and can lead to its failure.
Cooling a capacitor helps to enhance its performance as well as its reliability. Cooling will extend its life; taking away more heat from the capacitor can also give it more power-carrying ability.
Methods of Cooling Capacitors
The most common cooling methods include self-cooling, forced ventilation and liquid cooling. The simplest method for cooling capacitors is to provide enough air space around the capacitor so it will stay sufficiently cool for most applications.
“Most applications,” but not all. In many designs and installations self-cooling through natural air circulation simply cannot cool capacitors adequately. In higher power cases, the larger heat load may require additional cooling by means of an external heat dissipator or heat sink (not unknown, but not common with capacitors since they take up a lot of space); a fan, which can forcefully direct cooling air over the capacitor; or liquid cooling. Water-cooled capacitors are usually employed in applications such as induction heating, melting or annealing, as well as in high-frequency welding systems.
Here, losses in the form of heat are desirable. Induction heating, a controlled and contactless method of heating, takes place when an electrically conductive material is placed within a variable magnetic field. Induction heating finds applications in many industries for forging, welding, sealing, etc.
Induction heating is ideal for automated production lines and controlled environments – for example, the automotive industry uses induction for heat-treating a variety of chassis and drivetrain parts.
As induction heating experts will note, installing the proper cooling system will extend the life of an induction power supply, reducing maintenance costs and downtime. A typical induction heater system includes a power supply, impedance matching circuit, tank circuit and applicator. Choosing proper capacitance for the resonant circuit is important in designing a resonant induction heating system: the capacitance affects the resonant frequency, output power, ESR, Q-factor, heating efficiency and power factor.
The resonance tank in an induction heating system is normally a parallel set of capacitor and inductor which resonates at a certain frequency. A bank of capacitors provides the needed capacitance in order to reach a resonance frequency matching the capability of the power supply. The inductor is the source of electromagnetic energy.
In these applications, the system’s capacitors can reach temperatures that require liquid cooling. These water–cooled capacitors are specially designed for use in inductive heating and melting plants for power factor improvement and also for tuning of the circuits for varying inductive loads. The liquids that are commonly used in such systems are water, a mixture of water and chemical solutions, and de-ionized water.
As Anthony Kenny states in his article on the subject, “Most traditional cooling systems are designed to cool a capacitor by passing the cooling medium over the external casing of the component.” However, such methods of cooling (which only bring the cooling medium into contact with the external case of the capacitor) are not as efficient thermally as the designs of water-cooled capacitors where water is passed through the interior of the capacitor so that heat is extracted as close as possible to its where it is generated. In most modern water-cooled capacitors, the cooling medium passes through the interior of the component.
The cooling conditions in place will help determine the performance and operating lifespans of these water-cooled capacitors.
An Environmentally Correct Cooling System
Now that we’ve spent some time reviewing methods aimed at ensuring that the temperature of a capacitor is maintained within acceptable limits, let’s move on to an emerging capacitor-based technology that is showing promise as a “green” cooling agent.
Designs for what is known as electrocaloric (EC) cooling use materials that change temperature under an electric field, leading to a temperature difference between the hot side and the cold side. Multilayer ceramic chip capacitors (MLCCs) are promising EC cooling elements because they operate at low voltages, possess large breakdown fields, contain inner electrodes that facilitate heat transfer and exhibit sufficiently active EC material.
As Xavier Moya et al. note in their research, “the observation of electrocaloric effects in commercial multilayer capacitors has inspired the possibility of environmentally friendly cooling.” This type of cooling system boasts increased efficiency, with few or no moving parts and without the need for refrigerants that harm the environment or pose a fire hazard.
What is more, EC multilayer ceramic capacitors can be fabricated in a manufacturing-compatible process. Recently, a group of scientists from Xerox Parc described in the journal Science an EC cooling material employing lead, scandium and tantalum (PST) in multilayer ceramic capacitors that change temperature under an electric field.
These researchers obtained a system temperature span of 5.2 degrees C and a maximum heat flux of 135 milliwatts per square centimeter. They used a large-volume fabrication technique often employed in the electronics industry to produce a device from MLCCs that, the scientists say, shows how lab-scale devices that change temperature under an electric field could be scaled up.
When they applied an electric field of 10.8 MV/m, the capacitors underwent an adiabatic temperature rise (and fall) of 2.5 degrees C per cycle at room temperature. With the cold sink steadily cooling over the course of about 100 cycles, its temperature dropped by up 5.2 degrees C compared with the hot sink.
According to the researchers, the measured heat flux was reported to be more than four times higher than other EC cooling demonstrations, and the temperature lift was among the highest for EC systems that use ceramic multilayer capacitors, according to the researchers.
The device invented by the research team isn’t fully solid state. The electrocaloric effect involves alternately applying and removing an electric field to the material to increase and decrease the material's temperature, respectively. The PARC device has two layers of multi-layer capacitors lined up between copper rails and separated by insulators. The upper layer contains five capacitors, while the lower one has four and is capped by an aluminum heat sink at each end.
The device physically moves the capacitors back and forth between hot and cold regions to effect cooling. An actuator moves the top layer so that its capacitors are always aligned with those below, while an extra capacitor at either end comes into and out of thermal contact with the heat sink below it. Repeating this process results in cooling.
Multilayer capacitors of PST have been demonstrated to be well-suited for cooling applications. With further development, one day these electrocaloric cooling devices may even replace today's refrigerators and air conditioners.
Sources / Further Reading:
Anthony Kenny, “The Anatomy of a Water Cooled Capacitor”
RDO Induction, LLC, “Components of Induction Heating”
Xavier et al., “Electrocaloric effects in multilayer capacitors for cooling applications”
Wang et al., “A high-performance solid-state electrocaloric cooling system,” Science, 10.2.2020
Follow TTI, Inc. on LinkedIn for more news and market insights.
Statements of fact and opinions expressed in posts by contributors are the responsibility of the authors alone and do not imply an opinion of the officers or the representatives of TTI, Inc. or the TTI Family of Specialists.