Fort Worth, Texas – March 9, 2021 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of Gen 4 EV CCS Charging Inlets from stock today.
Phoenix Contact offers Gen 4 EV CCS Charging Inlets through TTI. The universal CHARX connect CCS Charging Inlets enable the AC and DC charging of electric cars and electric utility vehicles – from low charging powers all the way up to high power charging (HPC). These vehicle charging inlets were originally developed for leading manufacturers in the automotive industry and are already being used in the new generations of electric vehicles. They allow electric vehicles to be charged continuously with a power of 250 kW and temporarily up to 500 kW. They are IP6K9K and were developed in accordance with IATF 16949 and conform to IEC 62196, SAE J1772 and GB/T 20234.
To learn more, visit Phoenix Contact Gen 4 EV CCS Charging Inlets at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com.