Fort Worth, Texas – March 3, 2021 – TTI, Inc., a leading specialty distributor of electronic components, announces the availability of BergStak® 0.40mm Self-Alignment Board-to-Board Connectors from stock at TTI.
BergStak® 0.40mm Self-Alignment Connectors come with a stack height of 3.50mm and 30 positions extendable from to 10 to 60 positions with 10 positions incremental. It has a unique self-alignment feature that supports blind mating, ensuring a reliable connection. The USCAR-2 compliant connector is also ideal for the automotive market. Typical applications include car camera, portable IoT, factory automation and patient monitoring. They are in stock and available today at TTI.
To learn more, visit BergStak® 0.40mm Self-Alignment BtB Connector at TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.ttiinc.com.