Fort Worth, Texas – November 10, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking a wide range of TE Connectivity Industrial Relays.
TE Connectivity offers a full line of relay and contactors including leading brands such as AGASTAT, AXICOM, CII, HARTMAN, KILOVAC, OEG, P&B, PRODUCTS UNLIMITED and SCHRACK, as well as TE Connectivity. Switching capabilities range from dry circuit to 1,600A, up to 70kV, and as high as 6 GHz. Electromechanical, solid state and hybrid types range from surface-mount PCB mount devices to large panel mount units. The broad line of relays features expansive options for enclosure, termination, input, contact arrangement and rating. High performance types are designed specifically to operate in extremely rigorous environments (high shock, vibration, temperature, altitude) such as encountered in military and aerospace applications. For applications utilizing PCB and DIN rail-mounted versions in industrial environments, TE recommends the PT and the Force Guided series. Reference the Relay Products Catalog for the exact relay that will fit best for your application.
To learn more, visit TE Connectivity Industrial Relays at TTI
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com.
About TE Connectivity
TE Connectivity is a $13 billion global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions, proven in the harshest environments, enable advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With nearly 80,000 employees, including more than 8,000 engineers, working alongside customers in approximately 150 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com and on LinkedIn, Facebook, WeChat and Twitter.