Fort Worth, Texas – November 10, 2020 – TTI, Inc., a leading specialty distributor of electronic components, is now stocking an expanded offering of ROHM infrared components.
These infrared LEDs are suitable for many non-contact sensing applications especially for medical and industrial products. With automotive quality built in, they are well suited for medical equipment sensing needs like ECG/(EKG) equipment, pulse oximeters, digital stethoscopes, blood glucose meters, blood pressure monitoring and ultrasound systems.
ROHM also offers a variety of spectrally matched sensors in phototransistor and photodiode output configurations. These products are available in both through-hole and surface mount packages and are offered in wavelength ranges of 850nm – 870nm to fit your design requirements. This makes it possible to design in matched optical characteristics, significantly easing the design challenges.
Additionally, by optimizing the LED die, ROHM was able to improve intensity and overall reliability. Most of these LEDs are AEC-Q101 qualified, making them suitable for the ever-increasing medical equipment requirements.
View all ROHM Semiconductor products.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com.
About ROHN Semiconductor
ROHM offers a full line of leading-edge sensors, silicon carbide MOSFETs and Schottky barrier diodes, infrared optoelectronics, and power management ICs. If you’re designing for rugged environments requiring high-temperature and/or high-voltage along with higher power density solutions – TTI is fully franchised for ROHM, Kionix MEMS Sensors and accelerometers, and LAPIS Semiconductor products.