Fort Worth, Texas – November 9, 2020 – TTI, Inc., a leading specialty distributor of electronic components, announces the immediate availability of Micro-Fit+ Right Angle Headers from stock at TTI.
With its unique keying design, Micro-Fit+ Connectors offer up to 12.5A with a 3.00mm pitch, allowing it to deliver higher current capacity in the same space. Additional features include a smaller PCB footprint, a reduced mating force by 40% and an enhanced TPA design that provides stability and security for the terminals inside the receptacle. Target markets include consumer, telecoms, medical, sustainable energy and automotive, to name but a few. They are in stock and available today from TTI.
About TTI
TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of electronic components. Founded in 1971, the emphasis on a broad and deep product portfolio, available-to-sell inventory and sophisticated supply chain programs have established TTI as a distributor of choice to manufacturers in the industrial, defense, aerospace, transportation, medical, and communications sectors worldwide. TTI and its wholly owned subsidiaries, the TTI Family of Companies, Mouser Electronics, Sager Electronics and TTI Semiconductor Group employ over 7,000 people in more than 133 locations throughout North America, South America, Europe, Asia and Africa. Globally, the company maintains over 2 million square feet of dedicated warehouse space housing over 850,000 component part numbers. For more information about TTI, visit www.tti.com.