Fort Worth, Texas – December 13, 2018 – TTI, Inc., a leading specialty distributor of electronic components now stocks Phoenix Contact FKCOR and FKCOW Terminal Blocks. The push-in spring connection allows for quick and easy wire termination while color-coding ensures maximized mating accuracy. The connectors simplify wire rail management and are ideal for DIN rail-mounted devices. 

The FKCOR and FKCOW is available with screw flange, and lock and release lever system for a secure connection. They are rated up to 12 A and 300 V UL with a 5.08 mm pitch and 2 to 24 positions per connector for greater installation convenience. The connectors can be used in automation, energy technology, and distributed power applications.

To learn more visit https://www.ttiinc.com/content/ttiinc/en/manufacturers/p-s/phoenix-contact/products/right-angle-spring-contact-connectors.html

 

PHX-FXCOR_PR-Image

About TTI

TTI, Inc., a Berkshire Hathaway company, is an authorized, specialty distributor of interconnect, passive and electromechanical (IP&E) components and the distributor of choice for industrial and consumer electronics manufacturers worldwide. Broader and deeper inventory, leading-edge products and custom supply chain solutions have established TTI as the leading specialist in electronic component distribution. Globally, the company maintains 1.9 million square feet of dedicated warehouse space containing over 850,000 component part numbers. Along with its subsidiaries, Mouser Electronics, Sager Electronics, and TTI Semiconductor Group. TTI employs over 6,000 employees and is represented in over 100 locations throughout North America, Europe and Asia. For more information about TTI, visit www.ttiinc.com

 

About Phoenix Contact

 

Phoenix Contact is a globally present, Germany-based market leader. Our group is synonymous with future-oriented components, systems, and solutions in the fields of electrical engineering, electronics, and automation. A global network across more than 100 countries and 15,000 employees ensure close proximity to our customers, which we believe is particularly important. For more information about Phoenix Contact, visit www.phoenixcontact.com